N/A
Heating
> Heating
> News
> News Archive
> Balancing Valves
> Burner Components
> District Heating
> Floor Heating Electrical
> Floor Heating Hydronics
> Heat Pumps
> Radiator Thermostats
> Ventilation
 
 
 
 
 
Danfoss Logo
The SIB ZERO +House - an excellent example of Danfoss' wide range of professional and energy saving solutions put into practice

Danfoss Solutions used in SIB Zero +House

01 November 2009
The SIB ZERO +House is the name of Denmark's first low energy +house. The house, which was recently completed in the town of Sønderborg, has positive annual energy costs and provides a glimpse of tomorrow's energy efficient home.


The 200 m2 home actually produces more electricity than it consumes on an annual basis, which is why it is known as a +house. The excess energy is created through a unique combination of known technologies that turn the home's energy consumption into energy production. Danfoss contributed with solutions for the indoor climate and comfort system to this project, which includes the use of a Danfoss Air system and Danfoss fast acting floor heating.

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.